Unrivaled reliability and highly efficient. Mitsubishi Electric Uninterruptible Power Supply systems for maximum critical infrastructure protection.
Purpose-built and highly efficient. Mitsubishi Electric Cooling Systems for IT and electrical equipment.
Deliver consistent, reliable connectivity to your customers with an uninterruptible power supply for telecommunications. Mitsubishi Electric UPS keep your network up and running in the event of a power outage or disturbance.
Remote critical infrastructure with minimal personnel requires reliable telecom backup power for maximum uptime.
When communication is mentioned as a mission critical application, satellite systems and tall microwave towers come to mind. But, in today's marketplace, communications encompasses far more, including video conferencing, VoIP networks, 5G, and IoT. As customer demands for connection rise exponentially, failure of a communications network is simply not an option.
Advance infrastructure components in parallel to meet the changing demands and load requirements on your network.
With the evolution of telecommunications and ever-increasing customer demands, the industry is seeing a major shift from analog and wire to data centers, requiring you to digitize your critical infrastructure and enhance your design. In doing so, your required power rating will go up. There will be more data to manage, and you will need bigger servers. Your bigger servers will need larger, more reliable, and more technically sophisticated UPS and peripheral equipment.
Enter Mitsubishi Electric's telecom UPS options. Our UPS for internet, phone and other communications applications deliver the elevated telecom backup power that complex systems require, within a small footprint.
Emergency call centers can’t afford a break in communication. When connectivity is required to ensure the safety and security of others, uptime can be a matter of life and death.
For firefighters battling a raging inferno, presenting imminent danger to both residents and the emergency responders, a communications infrastructure must operate without compromise. Similarly, a paramedic assisting victims of a violent vehicle collision or assault needs to have reliable communication between the scene of the accident and the closest medical facility. In these situations, effective and reliable backup power systems are imperative, and a reliable UPS from Mitsubishi Electric will maintain network uptime.
Any network latency can be a major roadblock – especially if real-time processing is required. And even when it’s not – no customer likes to be kept waiting.
While not every call is an emergency, telecom companies need to ensure daily operation of their communications networks runs smoothly to keep up with increasing customer demands. In B2B communication situations, a degradation in service can cause service-level agreement penalties, low customer satisfaction, or loss of revenue.
Businesses and consumers alike expect continuous transmission and delivery of voice and video calls, texts and email, live broadcasts, information, and content over satellite, cable, and fiber. Telecom backup power needs to be able to keep your growing network intact despite power fluctuations and outages.
Whether supporting your centralized data center, regional office, or an edge data center, telecom backup power needs to be reliable and small in footprint. That’s just what you get with Mitsubishi Electric 3 phase UPS, with models available from 10kVA to 2000kVA.
Solutions from energy dense lithium-ion in LMO/NMC or SFLP chemistries to a range of lead acid batteries like 12V standard VRLA and advanced thin plate pure lead (TPPL) can support our UPS for internet and telecommunications applications. Our battery options are UL9540A tested to reduce thermal runaway and are designed to operate safely in a small footprint.
UScellular partnered with MDI Access to implement a variety of green initiatives, including installing SUMMIT Series® UPS to receive significant cost savings and substantial government rebates.
and more...
Continuous and clean telecom backup power is essential to ensure communications are seamlessly maintained during power outages and disturbances. If your telecom network is supported by a Mitsubishi Electric UPS, you will have the backup power you need to keep customers connected – whether backing up emergency call centers or calls to grandma. Make sure your emergency and standby power systems are supported by a reliable UPS.