Hero Component

This is the hero component set to full height. Transparent background color options include white, red, black and blue. On mobile copy falls below hero image. Copy block can be aligned right, center, left and top, middle, bottom. A optional CTA button can also be added to this component. 

Hero Component

This is the hero component set to full height. Transparent background color options include white, red, black and blue. On mobile copy falls below hero image. Copy block can be aligned right, center, left and top, middle, bottom. A optional CTA button can also be added to this component. 

adding new field for test

This is the Rich Text Editor Component in a two column medium width container. The component to the right is an image component. 

 

Here you can chose from pre-formatted fonts.

H1

h2

h2 with red line on top

h3

h3 subheader

h4

h5

h6

You can make any of these in red

  • You can use Gray
  • You can have small paragraph text

 

Watch Now

This is the YouTube embed component. Title and caption text are optional.

This is image with block overlay component.

 

Copy seen here can be formatted. 

 

Background color options include white, black, light gray, red and blue. 

 

CTA button can be added as an option.

Below is full width image component.

 

This container also has a light gray background applied.

Text block with Image

This component is similar to the text block component however offers the ability to add an image to the right or left of copy. 

 

Description copy can go here. 

test Photo

Text block

 

  • Copy can be formatted. 
  • Background color options are white, light gray, black, red and blue

 

This is in a single column small width container. 

 

 

Below is the Featured Items component. You can have up to six features at a time. Each feature allows the ability to add an image, title and optional link. 

 

Image with block overlay component in two column

Below are button component options available. These can all be set to small, normal, large, full width or full width mobile only. Full width, will be the width of the width of the column it is in. Buttons can be aligned right, center, left within the column.



This is a three column container. 

 

Image component below and video embed and rollover image component to the right. 

 

YouTube Embed Title

YouTube Embed

Four Column Container

Right Sidebar Container

 

Within this container you can use rich text, buttons, image and video embed components.

Left sidebar container

This is the looping background component

Here you can format copy. Copy block along with CTA can be right, center or left aligned. 

This is the looping background component

Here you can format copy. Copy block along with CTA can be right, center or left aligned. 

This is the Hero Video Modal

Description copy can be seen here.

Watch Now

This is the Hero Video Modal

Description copy can be seen here.

Watch Now

Video Title

YouTube embed in a single container. Copy is optional and pre-formatted.

Image With Block Overlay

 

This is the image with block overlay component. Here you can format copy. 

Thumbnail Image
Thumbnail Image
“ This is the quote component. Image is optional and can be placed to the right, left or on top of the quote. Copy is pre-formatted. ”

- Author, Author's Title

“ This is the quote component. Image is optional and can be placed to the right, left or on top of the quote. Copy is pre-formatted. ”

- Author, Author's Title