UPS for Energy Sector & Utility Providers

Energy and power suppliers are responsible for keeping the grid up for their customers. In the event of an outage that impacts the power plant, UPS can back up controls and operations so you're able to get the grid back up more quickly.

UPS for Energy Sector & Utility Providers

Energy and power suppliers are responsible for keeping the grid up for their customers. In the event of an outage that impacts the power plant, UPS can back up controls and operations so you're able to get the grid back up more quickly.

Power Plant UPS Keep the Lights on for Providers so they can deliver to customers

Many opportunities for power failure exist in the complex infrastructure that lies between a power plant and a simple wall socket.


You can reduce the chance of downtime and equipment damage with an uninterruptible power supply at the source, as well as downstream installations that keep relay stations up and running. 

 

Energy generated in power plants is transmitted great distances via overhead lines and distributed among scattered substations. Each substation employs numerous auxiliary equipment including transformers, circuit breakers, switchgear, relays, and SCADA systems performing a range of tasks depending on the locale's specific needs.

With UPS installation in plants and substations, you can guard against downtime throughout your entire infrastructure.

 

Even the Energy Sector Needs an Occasional Boost from UPS

Avoid the irony of a power plant without power with uninterruptible power supplies to ensure the continuity of the utility's supply and minimize disruptions.


UPS for utilities can provide the uptime you need to safely switch to a backup generator or power down without damaging equipment. Smaller, remote installations can back up the overall power distribution system and support on-going computerized operations in the substations so energy can continue to reach customers even during extreme conditions that trigger outages.

 

Power plant UPS are also used to provide an extra layer of protection for security alarms and communications in utilities and their respective network of remote substations.

UPS can help maintain control systems in power plants

Uninterruptible power supplies can offer protection to your equipment and essential service throughout your infrastructure.


Power plant UPS keep operations up while a UPS installed in an 811 call center can help keep lines open so utility lines aren't damaged by misinformed digging. Whatever point in your power distribution needs support, Mitsubishi Electric can help.

 

Energy and utility companies operating nuclear, natural gas, alternative, or electric power plants trust our UPS systems to protect their critical equipment and make sure they can support their customers downstream with power they need for smooth, everyday operations.

 

Suggested Products for Energy & Utility Power Suppliers

Avoid undesirable downtime and ensure reliable power distribution to users with an Uninterruptible Power Supply from Mitsubishi Electric. 

 

 

Three Phase UPS to satisfy your power requirements:

DiamondPlus® 1100A & 1100B UPS


120/208V / 10 to 80 kVA

 

9900AEGIS UPS


480V / 80, 100, 150, 160, & 225 kVA

 

9900B UPS


480V / 300, 500, & 750 kVA

 

SUMMIT Series® UPS


480V / 500 & 750 kVA

 

9900CX UPS


480V / 1MW (1050 kVA)

Energy Power Supply Case Studies

 

Call Before You Dig hotlines help protect utility lines from damage, maintain service and protect workers, so it's important the call centers handling questions have maximum uptime. A Mitsubishi Electric UPS helps keep PA One Call's lines accessible despite outages.

 

Trust the Experience of our Energy & Utility Sector Partners

 

“ Reliability is the most important factor when purchasing equipment to protect against power outages, and I haven't experienced a single problem with the first 1100. ”

- Bill Kiger, VP Sales and Operations, PA One Call

Learn More about Suggested UPS Products
for Energy & Utility Applications