Uninterruptible Power Supply Systems

UPS systems with unrivaled reliability and superior efficiency to ensure your business doesn’t go dark.

Uninterruptible Power Supplies

Industry-leading reliability from 6-2000kVA

Uninterruptible power supply failures remain the leading cause of power outages across the data center industry1. With the relentless demands on today’s mission critical facilities, selecting highly reliable – tested and proven – UPS equipment is critical.

 

Whether you operate a hyperscale data center that demands a power dense UPS or a network that needs a compact single-phase backup, Mitsubishi Electric’s UPS systems are designed to be resilient and robust, keeping your business from going dark.

“It’s extremely robust and, quite frankly, I have a lot less people coming to my site operating and maintaining them as opposed to other vendors’ equipment.”

– Cameron Wynne, Chief Data Center Officer at Element Critical

3 Phase UPS Systems: 10kVA – 2MW 

Ranging from 120/208V 10kVA to 480V 2MW, our three-phase UPS systems deliver clean, balanced power to your critical loads.

 


Single Phase UPS: 6-12kVA

Our single-phase system is the 7011B, commonly used to back up individual computers, standalone IT racks, or other applications with limited load (less than 10kVA). 

Mitsubishi Electric's single phase7011B UPS.

Mitsubishi Electric UPS Technology

Beginning with the use of IGBTs for converters and inverters and followed by 3-level topology and transformerless UPS designs, Mitsubishi Electric has long been at the forefront of offering uninterruptible power supplies with the highest efficiencies and unparalleled reliability.

 

Unparalleled Reliability

At 99.9995%, Mitsubishi Electric Uninterruptible Power Supplies achieve the highest equipment reliability among UPS suppliers, ensuring you – and your customers – are protected against downtime 24/7/365. We calculate our equipment reliability as the percentage of time our backup power systems have sustained their load carrying capacity. 

The reliability formula.

e = # of reported customer load loss events due to a Mitsubishi Electric UPS failure

d = Assumed maximum duration of load loss events

u = # of Mitsubishi Electric uninterruptible power supplies shipped

tn = Assumed total available operational hours of UPS n since shipment

By manufacturing and heavily testing the advanced power electronics used in our UPS systems, we possess intimate knowledge on how to control them. High speed sampling and switching deliver hyperscale performance and value –

  • Achieving the highest levels of efficiency under all load conditions
  • Increasing cost savings & longer product life from cooler operation
  • Possessing the flexibility to operate in higher temperatures
UPS capacitor tray and IGBT device.

Efficiency Across the Load Range

Our superior expertise in optimizing power device control is evident by the consistently high efficiency curves across our UPS product line.

 

Considering loads in data centers can range anywhere from 25% to 80%, demonstrating high efficiency across all load levels is a critical element of UPS reliability and performance.

9900D Efficiency Curve graph.

Online Double Conversion

Achieve clean, consistent power with online double conversion technology. By filtering and converting incoming AC power to DC and back to clean, stable AC, online double conversion UPS systems deliver reliable power conditioning to protect critical loads from transient or voltage anomalies.

 

Explore the differences between double conversion vs. line interactive.

Online double conversion UPS technology means you are fully protected.

UPS System Configuration & Redundancy

The complexity of each UPS configuration varies based on budget, uptime requirements, risk aversion, maintenance plans, and existing infrastructure. 

 

Mitsubishi Electric’s Project Application Engineering team will configure a customized critical backup power system, incorporating batteries, maintenance bypasses, paralleling gear, and more to support your application.

Diagram showing N+1 configuration.

UPS Testing & Quality

As a prerequisite for success, every UPS system from Mitsubishi Electric and furnished with a signed factory test report prior to shipment. Our clients are encouraged to view real-time data and results via a product demonstration or a factory witness test of their purchased system – a great opportunity to simulate on-site needs.

“It was really cool to be able to prop open the doors and see the inside and be given an explanation of what all the parts and pieces were and how they worked”

– Jonathan Markum, Logistics Project Engineer


UPS Systems for Mission Critical Applications

Applications where downtime can be catastrophic are where we thrive. Our robust technology is configured and heavily tested to ensure reliable backup power in the most demanding environments.

 

Critical Load Application Suggested UPS Models
Hyperscale, Colocation, & Enterprise Data Centers: Computing Workloads & Core Networks
Meet strict uptime at massive scale and follow through on your SLAs
Hyperscale, Colocation, & Enterprise Data Centers: Ancillary Workloads
Deliver reliable power to ancillary – but just as critical – workloads, such as cooling, PDUS, security systems, control rooms, and more
On Premise, Network, & Regional Edge Data Centers: Computing Workloads
Reduce latency issues and enable time-sensitive data processing
Medical Equipment
Patient care is your number one priority, making protecting patient care technology (MRI, CT scans) your number two priority.
Emergency Lighting
Ensure safe evacuation during emergency situations with a UL-924-listed UPS system
Manufacturing & Light Industrial
Power conditioning and reliable backup power to maximize the output of your product line.

Success Stories

“Mitsubishi Electric offers an exceptional balance of technical sophistication and value for what you get.”

– John Dumler, Vice President, Data Center Design & Engineering at DC BLOX

Complete Critical Backup Power Systems

The longer you’re down, the higher the cost. Our comprehensive line of critical infrastructure protection equipment spans beyond uninterruptible power supplies to batteries, maintenance bypasses, communication cards, and more – all backed by a knowledgeable team of engineers and responsive service personnel. Failure is simply not an option when your mission is critical. Build the solution you need and protect it with preventative maintenance services.

UPS System Resources

Technology Insights

FAQs About UPS Systems

 

The role of a UPS is to bridge the gap in time between the moment the utility power is lost and when the generator starts. This ensures that the protected loads do not see any loss in power and that there is a smooth transition between the two power sources.

Redundancy in a UPS can refer to either internal module redundancy or system level redundancy.

  • Internal redundancy is when there are additional power modules in a UPS that are available to carry the load in the case of a fault condition in another module.
  • System level redundancy is when there are multiple UPS in a system that are available to carry the load in the case of a fault in an entire UPS.

Learn more about the types of redundant systems.

The efficiency of a UPS is the ratio of the output power to the input power and shows the internal losses of the system.

 

Calculation: Efficiency = (Output Power / Input Power) x 10

For example, if the output power of the UPS is 100kW and the input power is 103kW the resulting efficiency is 97%.

 

Mitsubishi Electric has multiple energy-efficient UPS products to support your critical load. Currently, our most energy-efficienct UPS is the SUMMIT Series® (500 & 750kVA). The 9900AEGIS (80-225kVA) is also ENERGY-STAR rated.

Choosing the right size UPS is dependent on a variety of factors, from application to capacity needs, amongst others.

 

Here, we walk you through the basics of determining what size UPS is best to support your critical infrastructure: What Size UPS Do I Need? The Basics of Sizing a UPS 

  • An internal bypass is located inside the UPS itself and provides an alternate path for power to flow, “bypassing” the power electronics. The internal bypass, however, does not isolate the entire UPS, and power is still present at the input and output connections.
  • maintenance bypass is an external piece of equipment, typically containing circuit breakers, that provides an alternate path for power to flow around the entire UPS. This allows you to remove power at the input and output connections allowing technicians to safely perform work on the equipment.

In general, a UPS battery is an energy storage device that goes into effect when the critical utility power of a UPS system is offline. Then, the UPS switches to drawing power from the battery to keep critical loads online and running.

 

The UPS battery can be of a variety of DC technologies and/or energy storage devices, and it is a critical component of a UPS system.

 

Choosing a battery depends upon the UPS system’s specific use case. This use case depends on the technical, safety, and commercial requirements of the customer.

It is recommended to never run a UPS at 100% load capacity. Most are run at a 60-75% capacity. This can vary based on the design of the facility, type of load, and/or the redundancy of the system.

 

Learn more about the basics of UPS sizing.

Typically, a Mitsubishi Electric UPS has a design life of approximately 15 years.

  • Wondering whether you should repair, replace, or upgrade your UPS? Check out this quick read.
  • Wondering whether you should replace lifecycle parts or the whole UPS system? This article is for you!

UPS Summary Table

Mitsubishi Electric’s portfolio of uninterruptible power supply systems span single phase 6kVA to three phase 2MW. All our UPS systems are UL 1778-listed and feature online double conversion technology with equipment reliability of up to 99.9995% in the most demanding mission critical environments.

 

UPS Model Input Voltage Output kVA / kW Dimensions (in.) & Net Weight (lbs) Efficiency (AC to AC) Compatible Battery Types Peripherals Applications
7011B 208V

6kVA / 4.2kW

 

8kVA / 5.6kW

 

10kVA / 7.0kW

 

12kVA / 8.4kW

13.8”W x 29.9”D x 27.8”H — 298lbs

 

13.8”W x 29.9”D x 40.6”H — 496lbs

>91%
  • Internal VRLA batteries
  • External VRLA batteries
  • Maintenance Bypass Switch
  • CS141
  • RSAP
  • Individual Computers, Printers, Displays
  • Communications, Security, Point of Sale, & Security Systems
  • Website, Inventory Databases
  • Monitoring, Production, Test Labs, Simulators, Control Centers, & Power Conditioning (Light Industrial)
  • Network Towers
1100A 120/208V

10kVA / 9kW

 

20kVA / 18kW

 

30kVA / 27kW

 

40kVA / 36kW

 

50kVA / 45kW

19.7”W x 27.0”D x 55.1”H
290lbs (min.) to 730lbs (max.)
Up to 92.8%
  • VRLA
  • Pure Lead
  • Internal VRLA batteries (10 & 20kVA)
  • 3-breaker Maintenance Bypass with Transformer & Optional Distribution
  • 3-Breaker Maintenance Bypass with Optional Distribution
  • Standard Transformers
  • CS141
  • RSAP
  • Ancillary Loads in Hyperscale & Colocation Data Centers
  • Edge Computing
  • IT Closets / Server Rooms
  • Emergency Lighting (UL 924-listed)
  • Alarm, Communications, Point-of-Sale, & Security Systems
  • Inventory database, Elevators/Escalators, HVAC, ATMs
  • Monitoring, Production, Test Labs, Simulators, Control Centers, & Power Conditioning (Light Industrial)
  • Network Towers, Switchboards
  • Medical Equipment (MRI, CT scan)
1100B 120/208V

50kVA / 45kW

 

60kVA / 54kW

 

70kVA / 63kW

 

80kVA / 72kW

31.5”W x 27.0”D x 67.3”H
499lbs (min.) to 807lbs (max.)
Up to 93.1%
  • Lithium-ion
  • VRLA
  • Pure Lead
  • Wall-Mount, 3-breaker Maintenance Bypass
  • 3-breaker Maintenance Bypass with Transformer & Optional Distribution
  • 3-Breaker Maintenance Bypass with Optional Distribution
  • Standard Transformers
  • CS141
  • RSAP
  • Ancillary Loads in Hyperscale & Colocation Data Centers
  • Edge Computing
  • IT Closets / Server Rooms
  • Emergency Lighting (UL 924-listed)
  • Alarm, Communications, Point-of-Sale, & Security Systems
  • Inventory database, Elevators/Escalators, HVAC, ATMs
  • Monitoring, Production, Test Labs, Simulators, Control Centers, & Power Conditioning (Light Industrial)
  • Network Towers, Switchboards
  • Medical Equipment (MRI, CT scan)
9900AEGIS 480V

80kVA / 72kW

 

100kVA / 90kW

 

150kVA / 135kW

 

160kVA / 144kW

 

225kVA / 202.5kW

27.6”W x 32.8”D x 80.6”H — 772lbs

 

27.6”W x 32.8”D x 80.6”H — 860lbs

 

35.4”W x 32.8”D x 80.6”H — 1080lbs

Up to 96.6% (ENERGY STAR rated)
  • Lithium-ion
  • VRLA
  • Pure Lead
  • VLA
  • Floor-Mount 3-breaker Maintenance Bypasses (125-225A & 250-350A)
  • Floor-Mount 3-break Maintenance Bypasses with Transformer (125-250A & 350A)
  • Standard Transformers
  • Wall-Mounted DC Disconnects (15-400A & 500-800A)
  • Paralleling Gear (custom CLC)
  • CS141
  • RSAP
  • Web/SNMP/Modbus (LookUPS)
  • Ancillary Loads in Hyperscale & Colocation Data Centers
  • Computing Loads in Enterprise, Regional, or Network Edge Data Centers
  • Emergency Lighting (UL 924-listed)
  • Alarm, Communications, & Security Systems
  • Monitoring, Production, Test Labs, Simulators, Control Centers, & Power Conditioning (Light Industrial)
  • Medical Equipment (MRI, CT scan)
9900B 480V

300kVA / 300kW

 

500kVA / 500kW

 

750kVA / 750kW

55.1”W x 32.7”D x 80.7”H — 2360lbs

 

88.35”W x 32.7”D x 80.7”H — 3605lbs

 

106.9”W x 32.7”D x 80.7”H — 4525lbs

Up to 96.5%
  • Lithium-ion
  • VRLA
  • Pure Lead
  • VLA
  • Maintenance Bypasses (600A, 800A, & 1200-1600A)
  • Wall-Mounted DC Disconnects (700A Max & 1200A Max)
  • Paralleling Gear (custom CLC)
  • CS141
  • RSAP
  • Web/SNMP/Modbus (LookUPS)
  • Computing Loads in Enterprise & Regional Edge Data Centers
  • Medical Equipment (MRI, CT scan)

SUMMIT Series®

(ft. Silicon Carbide Power Electronics)

480V

500kVA / 500kW

 

750kVA / 750kW

79.4”W x 33.5”D x 80.4”H — 3072lbs

 

101.8”W x 33.5”D x 80.6”H — 4290lbs

Up to 98.2% (ENERGY STAR rated)
  • Lithium-ion
  • VRLA
  • Pure Lead
  • VLA
  • Maintenance Bypasses (800A & 1200-1600A)
  • Wall-Mounted DC Disconnect (1200A Max)
  • CS141
  • RSAP
  • Web/SNMP/Modbus (LookUPS)
  • Computing Loads in Colocation Data Centers
  • Computing Loads in Enterprise & Regional Edge Data Centers
  • Network Towers
9900CX 480V

1050kVA / 1000kW

118.1”W x 35.4”D x 80.7”H
6613lbs
Up to 97.0%
  • Lithium-ion
  • VRLA
  • Pure Lead
  • VLA
  • Maintenance Bypass (1600A)
  • DC Disconnect (1600-3000A)
  • Paralleling Gear (custom CLC)
  • RSAP
  • Web/SNMP/Modbus (LookUPS)
  • Computing Loads in Hyperscale & Colocation Data Centers
9900D 480V

1200kVA / 1200kW

 

1250kVA / 1250kW

133.9”W x 35.4”D x 80.7”H
7270lbs
Up to 97.0%
  • Lithium-ion
  • VRLA
  • Pure Lead
  • VLA
  • Maintenance Bypass (1600-3000A)
  • DC Disconnect (1600-3000A)
  • Paralleling Gear (custom CLC)
  • RSAP
  • Web/SNMP/Modbus (LookUPS)
  • Computing Loads in Hyperscale & Colocation Data Centers

Don’t Let Your Business Go Dark®

1Uptime Institute Global Data Center Survey 2025